PCA9450 without using I2C interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9450 without using I2C interface

Jump to solution
2,163 Views
Bata
Contributor II

Is it possible to operate the PCA9450 without using I2C?

If possible, please let me know the pin setting when not using I2C.
(e.g. SDAx and SCLx to GND, etc.)

Also, are there any restrictions other than the default settings due to not using I2C?

0 Kudos
Reply
1 Solution
2,155 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Kawabata-san,

If there is no need to reconfigure and monitor the status of the device during the operation, it is possible to operate it without I2C, there is no periodic watchdog required etc. like in other PMICs.

Having said that, we do not recommend this type of operation, even if there is no need to modify the default settings, having the ability to read the fault statutes etc. is often required and useful.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
2 Replies
2,156 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Kawabata-san,

If there is no need to reconfigure and monitor the status of the device during the operation, it is possible to operate it without I2C, there is no periodic watchdog required etc. like in other PMICs.

Having said that, we do not recommend this type of operation, even if there is no need to modify the default settings, having the ability to read the fault statutes etc. is often required and useful.

Best regards,

Tomas

0 Kudos
Reply
2,139 Views
Bata
Contributor II

Hi Tomas san

Thank you for your prompt reply.

I understood very much.

 

Best regards,

Kawabata

0 Kudos
Reply