PCA9450 without using I2C interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9450 without using I2C interface

ソリューションへジャンプ
2,107件の閲覧回数
Bata
Contributor II

Is it possible to operate the PCA9450 without using I2C?

If possible, please let me know the pin setting when not using I2C.
(e.g. SDAx and SCLx to GND, etc.)

Also, are there any restrictions other than the default settings due to not using I2C?

0 件の賞賛
返信
1 解決策
2,099件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Kawabata-san,

If there is no need to reconfigure and monitor the status of the device during the operation, it is possible to operate it without I2C, there is no periodic watchdog required etc. like in other PMICs.

Having said that, we do not recommend this type of operation, even if there is no need to modify the default settings, having the ability to read the fault statutes etc. is often required and useful.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,100件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Kawabata-san,

If there is no need to reconfigure and monitor the status of the device during the operation, it is possible to operate it without I2C, there is no periodic watchdog required etc. like in other PMICs.

Having said that, we do not recommend this type of operation, even if there is no need to modify the default settings, having the ability to read the fault statutes etc. is often required and useful.

Best regards,

Tomas

0 件の賞賛
返信
2,083件の閲覧回数
Bata
Contributor II

Hi Tomas san

Thank you for your prompt reply.

I understood very much.

 

Best regards,

Kawabata

0 件の賞賛
返信