NXP's PMIC recommendation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP's PMIC recommendation

ソリューションへジャンプ
5,266件の閲覧回数
shai_b
Senior Contributor II

Dear team,

I do have a customer who needs a tiny PMIC component (under 3X3mm) with a default DC/DC buck out of 1.2v with at least 200mA and there should be another DC/DC buck output with 1.8v and LDO of 3.3v (up to 100mA),

the minimum output needs are two DC/DC buck (for 1.2v and 1.8v ~200mA) and one LDO (3.3V for MCU and Sensors)

Could you please advise any recommendation for suitable PMIC from NXP selection?

BTW, the PCA9420 was selected and the beginning of the design, but due to fact that the pmic starts with a value of 1v on the DC/DC buck (by default) and not 1.2v the customer could not start his FPGA and can not configure the outputs as needed. maybe the PCA9460 could be suit but I do not have the full datasheet in order to know what are the default setting/outputs

Waiting for your kind feedback, thanks in advance.

KR,

Shai 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
5,246件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Shai,

yes, the samples for the PCA9460 should be available. Unfortunately I don't have an access to them. Please ask your direct contact in NXP for the samples. The CSR (Customer Sales Representative).

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
5,261件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Shai,

the PCA9460 is indeed suitable for your customer's application. Buck1 is by default 1.8V and all Buck and LDO regulators are ON by default. 

JozefKozon_0-1634017212392.pngJozefKozon_1-1634017251166.png

The PCA9460 datasheet is confidential and I am not allowed to share it here. Please create a ticket here and me or one of my colleague will share the PCA9460 with you. Or please download the datasheet from this link. 

JozefKozon_2-1634017514416.png

With Best Regards,

Jozef

0 件の賞賛
返信
5,254件の閲覧回数
shai_b
Senior Contributor II

@JozefKozon Hello,

That's such great news the PCA9460C looks ideal solution, could you please advise if there is a sample available?

BTW, I already requested the datasheet and I am waiting for your approval.

Thanks and regards,

Shai  

0 件の賞賛
返信
5,247件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Shai,

yes, the samples for the PCA9460 should be available. Unfortunately I don't have an access to them. Please ask your direct contact in NXP for the samples. The CSR (Customer Sales Representative).

With Best Regards,

Jozef

0 件の賞賛
返信
5,239件の閲覧回数
shai_b
Senior Contributor II

@JozefKozon, Thank you so much.

Could you please advise when I will get the full datasheet (It already has passed 48 hours when I have requested)?

my email is: [email protected]

Waiting for your kind help, Thanks a lot.

Regards,

Shai

タグ(1)
0 件の賞賛
返信
5,234件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Shai,

I have successfully downloaded the datasheet from the link. But unfortunately I am not allowed to share confidential documents here on the community. We are also not allowed to share our email addresses with customers. If I would send you the datasheet directly, I would violate it. Please create a new case here and me, or one of my colleagues will share the datasheet with you. I believe this is the fastest way.

With Best Regards,

Jozef

0 件の賞賛
返信