Maximum force for applying heatsink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum force for applying heatsink

ソリューションへジャンプ
1,081件の閲覧回数
jeroenvanandel
Contributor I

What is the maximum force for the following components:

PMIC:  PCA9450CHNY & PCA9450AAHNY:  56 HVQFN  package

0 件の賞賛
返信
1 解決策
1,062件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

We do not specify a maximum heatsink mounting force. We recommend to use thermal vias and a large ground pad under the EP to spread heat to the PCB. This is the primary intended method for thermal dissipation. If in your application a heatsink must be mounted on top, JEDEC recommends ≤20N for small QFN packages.

BRs, Tomas

元の投稿で解決策を見る

1 返信
1,063件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

We do not specify a maximum heatsink mounting force. We recommend to use thermal vias and a large ground pad under the EP to spread heat to the PCB. This is the primary intended method for thermal dissipation. If in your application a heatsink must be mounted on top, JEDEC recommends ≤20N for small QFN packages.

BRs, Tomas