MMPF0100F9 Table blank

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100F9 Table blank

Jump to solution
4,818 Views
peterhauck
NXP Employee
NXP Employee

I am using MMPF0100F9ANESR2 but there is only a “-“listed in the table for VGEN1_SEQ register. see page 18 section 6.1.1, table 10. All the power on sequences are given besides VGEN1_SEQ register. I cannot find any reference. Is there a reason why its missing or blank? https://www.nxp.com/docs/en/data-sheet/MMPF0100.pdf

0 Kudos
Reply
1 Solution
4,623 Views
yasuomisakyu
NXP Employee
NXP Employee

Hi Peter, 

For F9 OTP configuration, VGEN1 is not assigned in power-sequence. It is off by default and can be turned on by I2C after RESETBMCU is released. 

Regards,

Yasu

View solution in original post

0 Kudos
Reply
3 Replies
4,624 Views
yasuomisakyu
NXP Employee
NXP Employee

Hi Peter, 

For F9 OTP configuration, VGEN1 is not assigned in power-sequence. It is off by default and can be turned on by I2C after RESETBMCU is released. 

Regards,

Yasu

0 Kudos
Reply
4,623 Views
calibronic
Contributor III

Dear Yasuomi Sakyu

I am going to design a board based on i.MX6QP and MCIMX6QP-SDB as a reference design.

I have been checking the MCIMX6QP-SDB “i.MX6 SMART DEVICE SYSTEM” evk schematics.

It is used PMIC with MMPF0100F9AZES part nember. It is non-programmed part. I haven't access to socket programmer.
Can I used this part number MMPF0100F9ANES which has F9 pre-programmed configuration instead of MMPF0100F9AZES ?

0 Kudos
Reply
4,622 Views
jinyuzhang
NXP Employee
NXP Employee

Hi

Both MMPF0100F9AZES and MMPF0100F9ANES are pre-programmed sample with the same F9 configuration. MMPF0100F9AZES is automotive grade and MMPF0100F9ANES is industrial grade. Both device can be operated up to Ta 105degC.

BRs

jinyu

PMIC and SBC question
0 Kudos
Reply