MC33774ASP1AE & S32K311NHT0MPAST Interfacing example code with SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33774ASP1AE & S32K311NHT0MPAST Interfacing example code with SPI

1,561 Views
db_1008
Contributor I

For 18 cell Lithium Ion BMS , using MC33774ASP1AE & S32K311NHT0MPAST . Is there any example code of interfacing the MCU with AFE on SPI?

Found this MC33774A Communication - NXP Community, but its on S32K344, is there any example code for testing on  MC33774ASP1AE & S32K311NHT0MPAST ?

0 Kudos
Reply
3 Replies

1,527 Views
db_1008
Contributor I

Dear Jozef,

Thanks for info.

I could see one reply on this post with code attachement : MC33774A Communication - NXP Community

Is it removed, or did it had any bug in it?

0 Kudos
Reply

1,523 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Deepak,

I don't see any answer either in the MC33774A Communication - NXP Community. It was probably removed. 

With Best Regards,

Jozef

0 Kudos
Reply

1,542 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Deepak,

We currently do not have examples for the S32K311 direct SPI with the MC33774A. At this time, our evaluation boards do not support direct SPI communication with the MCU. This boards with MC33774A are designed exclusively for TPL (isolated daisy chain) communication and cannot be used for SPI communication.
To interface between SPI and TPL, a gateway such as the FRDM665SPIEVB is required. Unfortunately, the  software for direct communication between the S32K311 and the MC33774A have not been developed.

I apologize for any inconvenience.

With Best Regards,

Jozef

0 Kudos
Reply