How to download program in normal mode(not in debud mode)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to download program in normal mode(not in debud mode)?

7,485 Views
dingsg
Contributor I

hi !

     I have a question about FS65xx  when I download  program.when I use  FS65xx to supply  power MCU in normal mode(not in debug mode),if i want to downloade a new program  by using  bootloader ,what should  i do?    And now I use IO port to pull up DEBUG pin in bootloader ,and release it in APP when download process is finished. Because I don't want to feed dog in download process.  How should  I operate FS65 in bootloader and it will meet functional safety  requirments.

Thanks!

Labels (1)
0 Kudos
Reply
14 Replies

7,339 Views
guoweisun
NXP TechSupport
NXP TechSupport

What kind of MCU platform do you select in your system?

0 Kudos
Reply

6,934 Views
xupei
Contributor I

Hello,

After reading it, I still don't understand the title question。

How to download program in normal mode(not in debud mode,e.g thru CAN )?thanks

"The watchdog refresh can be disabled during INIT_FS state of the fail-safe logic to allow programming without taking care of the watchdog refresh. INIT_FS can be entered by a reset request with RSTB_REQ bit in SF_OUTPUT_REQUEST register."The above is described in the guideline.

0 Kudos
Reply

7,339 Views
dingsg
Contributor I

Hi !

There are two kinds of MCU Platform,  they are MPC5775E and Infineon Aurix TC38x.

When using the two platforms, is there any difference in the function usage of fs65 ?

Thanks!

0 Kudos
Reply

7,339 Views
guoweisun
NXP TechSupport
NXP TechSupport

This is MCU MPC5775 related questions,I send your driver code based on MPC5774 platform, hope could help you!

0 Kudos
Reply

7,339 Views
dingsg
Contributor I

Thank you for your reply!

            I have a question ,Could you tell me if we need to feed watchdog when  we download the program? if needn't ,how should we deal with the Debug pin?

0 Kudos
Reply

7,339 Views
guoweisun
NXP TechSupport
NXP TechSupport

Download program in debug mode,no need to feed watchdog.

0 Kudos
Reply

7,339 Views
dingsg
Contributor I

  When fault occurs  ,  it can only be cleared by watchdog refresh ?

0 Kudos
Reply

7,338 Views
guoweisun
NXP TechSupport
NXP TechSupport

你说的什么种类的错误?

0 Kudos
Reply

7,339 Views
dingsg
Contributor I

过压故障产生后故障错误计数器会增加,这时候应该怎么清除故障呢

0 Kudos
Reply

7,339 Views
guoweisun
NXP TechSupport
NXP TechSupport

你的电话是多少?

0 Kudos
Reply

7,339 Views
dingsg
Contributor I

你好!我们在第一次烧写程序的时候,这时候即不能通过MCU去控制debug引脚,也不能实现正常喂狗,应该如何做操呢?

0 Kudos
Reply

7,339 Views
guoweisun
NXP TechSupport
NXP TechSupport

这样只能自己做外围的电路,上电默认满足进入debug模式

0 Kudos
Reply

7,339 Views
dingsg
Contributor I

座机电话:021-34978900 转 8740

手机号码:15821852057

0 Kudos
Reply

7,339 Views
dingsg
Contributor I

When we download program ,we use IO port to pullup Debug pin and release the pin in application  after download process has been finished, Does this approach meet functional safety requirements?

0 Kudos
Reply