How to control the PWM output of the FS23 HSx pins?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to control the PWM output of the FS23 HSx pins?

885件の閲覧回数
gumu
Contributor V

Hello,

 In our project, HSx is configured to drive LED lights, with four HS outputs, selecting PWM1, PWM2, PWM3, and PWM3 sources, at a frequency of 200 Hz. During debugging, we found that the interface Sbc_fs23_SetHSxSource() cannot control the corresponding channel's on and off ; instead, we need to use the interface Sbc_fs23_SetTimerPwm() to control them. Below is the configuration of the High side driver:

gumu_0-1731569709212.png

Additionally, read the configuration registers again , FS0B and LIMP pin levels high, everything is normal. I would like to ask if this control method is correct.

Thanks!

0 件の賞賛
返信
2 返答(返信)

791件の閲覧回数
gumu
Contributor V

Hi @quangvuanh,

I would like to ask if there is any result regarding this issue now?

Thanks!

0 件の賞賛
返信

874件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Quang (@quangvuanh),

Could you please help with this question from Anhui Zhitu Technology China?

Thanks & BRs, Tomas

0 件の賞賛
返信