FS8630 Safety manual SIR implement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS8630 Safety manual SIR implement

1,659 Views
CharlieYe
Contributor I
 

Screenshot 2025-03-10 165936.png

For system integrator, we don't need care and implement the SM38,SM42,SM43, because these safety mechanism is detected automatically. Also these safety mechanism don't any SIR in safety manual. 

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

1,642 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Charlie,

Yes, these safety mechanisms are detected automatically, meaning no additional implementation is required from the system integrator. They do not have associated SIR – implying that they do not require explicit integration efforts from the system perspective.

BRs, Tomas

0 Kudos
Reply

1,626 Views
CharlieYe
Contributor I
Hi Tomas,

Thanks a lot for your professional feedback, i understand how to choose the safety mechanism to implement.
And i also find that some SIR is not mapping to SM in safety manual. If it is necessary for system integrator to implement these SIR, such as SIR_07 of chapter 5.1.4 I2C commination. SIR_07 has no impact to SM39. SIR_07:It is the responsibility of of the system integrator to enable secure write function on I2C communication.
0 Kudos
Reply

1,610 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Charlie,

Since SIR_07 is a system-level responsibility, you must implement measures to ensure secure I2C communication beyond what PF502x does automatically. The lack of direct mapping to an SM does not mean it can be ignored. Instead, it requires active integration effort.

BRs, Tomas

0 Kudos
Reply