FS85xx: Behaviour when trying to close INIT_FS with a wrong WD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FS85xx: Behaviour when trying to close INIT_FS with a wrong WD

跳至解决方案
1,103 次查看
AndreasStolze
Contributor IV

Hi all,

quick question: What happens, if the challenger WD is used, and a bad WD is sent during trying to close the FS_INIT?

AndreasStolze_0-1712311440174.png

There's the WD_ERR_LIMIT, but is it also applied here?

Currently we're seeing a direct assertion of the RSTB pin but want this to be confirmed.

Also regarding debug mode:

Would be behaviour here be identical? Also a instant reset when the wrong WD is sent?

AndreasStolze_1-1712311600182.png

 

Thank you
Andreas

0 项奖励
回复
1 解答
1,086 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Andreas,

Yes, if there is no WD refresh or a bad WD refresh is sent during the INIT_FS phase, RSTB pulse is generated, the fault error counter is incremented by 1 and a new initialization phase is automatically started when RSTB is released.

No, in Debug mode, the INIT_FS window is infinite and the WD window is fully opened meaning WD errors are not taken into account.

BR, Tomas

在原帖中查看解决方案

2 回复数
1,087 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Andreas,

Yes, if there is no WD refresh or a bad WD refresh is sent during the INIT_FS phase, RSTB pulse is generated, the fault error counter is incremented by 1 and a new initialization phase is automatically started when RSTB is released.

No, in Debug mode, the INIT_FS window is infinite and the WD window is fully opened meaning WD errors are not taken into account.

BR, Tomas

1,083 次查看
AndreasStolze
Contributor IV

Thanks! Quick question, quick answer!

0 项奖励
回复