FS85 Debug mode: dumb mode possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS85 Debug mode: dumb mode possible?

Jump to solution
2,113 Views
AndreasStolze
Contributor IV

Hi,

as far as I understand the FS85 data sheet, in debug mode the FS85 will not turn on its regulators.

I guess if you use the KITFS85SKTEVM you can create a dummy OTP config and work with that (turning on the regulators).

However, if the FS85 is in a custom circuit, is there a way to just turn it on with its OTP configured regulator voltages? No watchdog or soever?
This would be very helpful for the board bring-up.

Thanks
Andreas

Labels (1)
0 Kudos
Reply
1 Solution
2,099 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can see below debug flow chart, in debug mode if you do the OTP or emulation to turn on regulators, then regulators will power up according OTP/emulation configuration :

guoweisun_0-1705369797253.pngguoweisun_0-1705369797253.png

 

View solution in original post

0 Kudos
Reply
2 Replies
2,090 Views
AndreasStolze
Contributor IV

Thanks for clearing that up @guoweisun 

Apparently we didn't do the right steps for debug mode. But now it works!

0 Kudos
Reply
2,100 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can see below debug flow chart, in debug mode if you do the OTP or emulation to turn on regulators, then regulators will power up according OTP/emulation configuration :

guoweisun_0-1705369797253.pngguoweisun_0-1705369797253.png

 

0 Kudos
Reply