FS6500 - INTERNAL RESET CIRCUITRY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6500 - INTERNAL RESET CIRCUITRY

1,956 Views
AnneVilasini
Contributor I

Hi ,

My query is regarding the internal reset circuitry used in SBC FS6500.

1. What is the maximum reaction time Trr of the reset ?

2. What is the maximum voltage drop that can occur during Trr max ?(indicated by delta U in the picture)

3.What is the minimum threshold voltage Vrt, which triggers a reset from the reset circuitry? (indicated by Vrt min in the picture)

4. What is the minimum voltage Vdd, which ensures the ECU does not reset?

AnneVilasini_0-1606796992538.png

 

0 Kudos
Reply
2 Replies

1,950 Views
guoweisun
NXP TechSupport
NXP TechSupport

1. What is the maximum reaction time Trr of the reset ?

overvoltage is the maximum reaction time 83uS;

2. What is the maximum voltage drop that can occur during Trr max ?(indicated by delta U in the picture)

It depends on output capacitor and loads after regulators.

3.What is the minimum threshold voltage Vrt, which triggers a reset from the reset circuitry? (indicated by Vrt min in the picture)

If UV configured as RSTB impacted, it is min UV threshold that can be found in the datasheet

4. What is the minimum voltage Vdd, which ensures the ECU does not reset?

it corresponding to the max UV threshold that can be found in the datasheet.

0 Kudos
Reply

1,940 Views
AnneVilasini
Contributor I

Hi Guoweisen, 

Thanks for your reply, 

Could you also please let me know , how the maximum reaction time of reset is considered as 83us?

 

0 Kudos
Reply