FS6500 Fuse Operation and configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6500 Fuse Operation and configuration

2,794 Views
mnewton
Fresh Out Contributor

The FS6500 Safety Mnaual refers to

"When the device is powered up, the fuses are loaded into a register bank, to fine tune internal electrical parameters, and checked by means of a hamming code."

However I can find no further information on the fuses or their operation. Are these NXP manufacturing fuses, not intended for developer modification? Is any configuration other than DEBUG MODE required for virgin board bring up?

Tags (2)
0 Kudos
Reply
2 Replies

2,673 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mike,

Yes, the fuses are not intended for developers‘ modifications.

 

No, only the Debug mode is recommended to be used when the SBC + MCU are powered first time to enable programming of the flash memory. In the Debug mode, the watchdog timeout is disabled by default, so there is no need to refresh the SBC watchdog periodically.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

2,557 Views
qiaoqin_wang
Contributor III

hello Tomas

i want to know how i to configure the debug mode from the hardware configuration and how to exit the mode ?

thanks for your help.

0 Kudos
Reply