FS5600 OTP regeisters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS5600 OTP regeisters

Jump to solution
1,988 Views
bwp530
Contributor IV

we have a MFS5600AMBA0ES on our board.

the datasheet says it is Non-programed.  

bwp530_0-1698670207743.png

this chip must be OTP programed? Does the SW1 and SW2 have voltage output? Does it have a default OTP configuration?

 

 

 

 

 

Tags (2)
0 Kudos
Reply
1 Solution
1,979 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is a blank device that needs to be programmed typically using our KITFS5600SKTEVM and the dedicated GUI according to the instructions in chapter 7.3 (OTP programming a blank device) of our UM11642.

SW1 output voltage is set via OTP_SW1_VOLT[7:0] bits and SW2 output voltage using OTP_SW2_VOLT[5:0] bits.

BR, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
1,980 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is a blank device that needs to be programmed typically using our KITFS5600SKTEVM and the dedicated GUI according to the instructions in chapter 7.3 (OTP programming a blank device) of our UM11642.

SW1 output voltage is set via OTP_SW1_VOLT[7:0] bits and SW2 output voltage using OTP_SW2_VOLT[5:0] bits.

BR, Tomas

0 Kudos
Reply