FS5600 OTP regeisters

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FS5600 OTP regeisters

跳至解决方案
1,204 次查看
bwp530
Contributor IV

we have a MFS5600AMBA0ES on our board.

the datasheet says it is Non-programed.  

bwp530_0-1698670207743.png

this chip must be OTP programed? Does the SW1 and SW2 have voltage output? Does it have a default OTP configuration?

 

 

 

 

 

标记 (2)
0 项奖励
回复
1 解答
1,195 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is a blank device that needs to be programmed typically using our KITFS5600SKTEVM and the dedicated GUI according to the instructions in chapter 7.3 (OTP programming a blank device) of our UM11642.

SW1 output voltage is set via OTP_SW1_VOLT[7:0] bits and SW2 output voltage using OTP_SW2_VOLT[5:0] bits.

BR, Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,196 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is a blank device that needs to be programmed typically using our KITFS5600SKTEVM and the dedicated GUI according to the instructions in chapter 7.3 (OTP programming a blank device) of our UM11642.

SW1 output voltage is set via OTP_SW1_VOLT[7:0] bits and SW2 output voltage using OTP_SW2_VOLT[5:0] bits.

BR, Tomas

0 项奖励
回复