FS4500 wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS4500 wake up

Jump to solution
10,428 Views
ydygcvjhbjkjnkn
Contributor I

Asking for help,
1. I want to know whether it is only necessary to call the SPI instruction to set the GO_LPOFF bit to 1 when setting the FS4500 sleep mode. After the SPI instruction is written successfully, the code running phenomenon will stop executing the subsequent code.
2. Given that the INH pin of 1145 transceiver is connected to IO_0 of FS4500, if you want to use 1145 transceiver to wake up FS4500 from LPOFF, do you only need to use the host computer to send CAN packet to wake up 1145 transceiver? The INH pin of the 1145 transceiver automatically affects the IO_0 of the FS4500 to wake up the FS4500. Can the subsequent code be continued, or does another method be required to wake up the FS4500?
Asking for help

0 Kudos
Reply
1 Solution
10,396 Views
guoweisun
NXP TechSupport
NXP TechSupport

1. I want to know whether it is only necessary to call the SPI instruction to set the GO_LPOFF bit to 1 when setting the FS4500 sleep mode. After the SPI instruction is written successfully, the code running phenomenon will stop executing the subsequent code.

[GW]看我标出来的箭头两个方式进入sleep的模式。

guoweisun_0-1744859427426.png

guoweisun_1-1744859529149.png

DFS要不要进入看上面的SELECTpin设定

 


2. Given that the INH pin of 1145 transceiver is connected to IO_0 of FS4500, if you want to use 1145 transceiver to wake up FS4500 from LPOFF, do you only need to use the host computer to send CAN packet to wake up 1145 transceiver? The INH pin of the 1145 transceiver automatically affects the IO_0 of the FS4500 to wake up the FS4500. Can the subsequent code be continued, or does another method be required to wake up the FS4500?

[gw]你是想通过1145的INHpin唤醒FS45吗从LPOFF模式?可以看下面圈出来的唤醒方式,如果是通过IO唤醒在进入sleep之前就要设定好,你要看不同模式下1145 INH的状态是不是符合唤醒的要求从而决定要不要1145 进入低功耗模式,逻辑很清楚需要您自己去设计这个功能

guoweisun_3-1744859800086.png

 

guoweisun_2-1744859687804.png

 

View solution in original post

0 Kudos
Reply
16 Replies
10,396 Views
guoweisun
NXP TechSupport
NXP TechSupport

1. I want to know whether it is only necessary to call the SPI instruction to set the GO_LPOFF bit to 1 when setting the FS4500 sleep mode. After the SPI instruction is written successfully, the code running phenomenon will stop executing the subsequent code.

[GW]看我标出来的箭头两个方式进入sleep的模式。

guoweisun_0-1744859427426.png

guoweisun_1-1744859529149.png

DFS要不要进入看上面的SELECTpin设定

 


2. Given that the INH pin of 1145 transceiver is connected to IO_0 of FS4500, if you want to use 1145 transceiver to wake up FS4500 from LPOFF, do you only need to use the host computer to send CAN packet to wake up 1145 transceiver? The INH pin of the 1145 transceiver automatically affects the IO_0 of the FS4500 to wake up the FS4500. Can the subsequent code be continued, or does another method be required to wake up the FS4500?

[gw]你是想通过1145的INHpin唤醒FS45吗从LPOFF模式?可以看下面圈出来的唤醒方式,如果是通过IO唤醒在进入sleep之前就要设定好,你要看不同模式下1145 INH的状态是不是符合唤醒的要求从而决定要不要1145 进入低功耗模式,逻辑很清楚需要您自己去设计这个功能

guoweisun_3-1744859800086.png

 

guoweisun_2-1744859687804.png

 

0 Kudos
Reply
10,377 Views
ydygcvjhbjkjnkn
Contributor I
感谢你的回答,我还想确认下,
1、在使用SPI指令设置寄存器GO_LPOFF设置为1后,代码此时停止运行是否是正常的
2、从手册中获取到不管当前的状态处于LPOFF—sleep还是Deep fail safe,都是可以通过IO_0唤醒,在使用SPI指令设置FS4500 进入低功耗时前,已将1145设置进入睡眠模式,并且FS4500的寄存器WU_IO0_1:0已经设置成01,除此之外还需要什么操作吗,然后使用上位机发送CAN报文唤醒1145,现象:不能够使FS4500退出低功耗,代码不能够继续运行起来
0 Kudos
Reply
10,367 Views
guoweisun
NXP TechSupport
NXP TechSupport

1、在使用SPI指令设置寄存器GO_LPOFF设置为1后,代码此时停止运行是否是正常的

【gw】看下面的描述进入sleep以后 MCU都没电了

guoweisun_0-1744869668608.png

 

 


2、从手册中获取到不管当前的状态处于LPOFF—sleep还是Deep fail safe,都是可以通过IO_0唤醒,在使用SPI指令设置FS4500 进入低功耗时前,已将1145设置进入睡眠模式,并且FS4500的寄存器WU_IO0_1:0已经设置成01,除此之外还需要什么操作吗,然后使用上位机发送CAN报文唤醒1145,现象:不能够使FS4500退出低功耗,代码不能够继续运行起来

【gw】在进入sleep以后,你有抓到测试到INH的电压变化吗波形?

guoweisun_1-1744870395977.png

 

0 Kudos
Reply
10,363 Views
ydygcvjhbjkjnkn
Contributor I
有测试1145的INH引脚,在初始进入低功耗模式时,使用万用表测试为0,使用上位机发送报文后,再次测试INH的引脚为12v
0 Kudos
Reply
10,360 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1744872220744.png

这个配置唤醒的口是在初始化INIT的阶段配置的不是在normal下配置的

你在初始化阶段动过这个寄存器吗?

guoweisun_1-1744872278208.png

 

0 Kudos
Reply
10,328 Views
ydygcvjhbjkjnkn
Contributor I
我现在测试到一种现象,
1、在1145收发器初始化进入睡眠模式之后,测量1145的INH引脚为低电平,测试FS4500的IO_0引脚此时是低电平(此时是正确的),
2、然后FS4500执行初始化流程,FS4500变成normal模式,测量1145的INH引脚为低电平,测试FS4500的IO_0引脚此时是低电平(此时是正确的),
3、通过SPI指令设置FS4500进入睡眠模式后(只是修改寄存器GO_LPOFF设置为1),此时测量1145的INH引脚为高电平,测试FS4500的IO_0引脚此时是高电平,当前没有对使用上位机发送任何报文,这个是为什么,不过代码现象还是停止执行后续代码,
0 Kudos
Reply
10,325 Views
guoweisun
NXP TechSupport
NXP TechSupport

第三步你把1145 INH断开,再看看到地是SBC IO0 是高的还是INH是高的,如果你没有操作1145任然在sleep下。

0 Kudos
Reply
10,322 Views
ydygcvjhbjkjnkn
Contributor I
我现在用的板子是好几层的,他们之间的走线在中间,不太好断开,根据手册,IO_0应该就是输入,不明确SPI操作FS4500指令进入睡眠模式,为什么会影响到1145的INH输出
0 Kudos
Reply
10,298 Views
guoweisun
NXP TechSupport
NXP TechSupport

你可以查看1145的状态通过寄存器查看下,看看目前是在哪个状态。

guoweisun_0-1744895307781.png

 

0 Kudos
Reply
10,290 Views
ydygcvjhbjkjnkn
Contributor I
谢谢你的回答,我现在找到问题的原因了
0 Kudos
Reply
10,285 Views
guoweisun
NXP TechSupport
NXP TechSupport

那是什么原因导致的?

0 Kudos
Reply
10,274 Views
ydygcvjhbjkjnkn
Contributor I
1145的wake引脚导致的
0 Kudos
Reply
10,406 Views
guoweisun
NXP TechSupport
NXP TechSupport

请问你们是什么公司啊?有网址吗?

0 Kudos
Reply
10,403 Views
ydygcvjhbjkjnkn
Contributor I
你好,公司网址
https://gkanghui.com/
0 Kudos
Reply
10,419 Views
guoweisun
NXP TechSupport
NXP TechSupport

请问您是哪个公司?能否用公司的邮箱提问呢?

因为用个人邮箱我们处理起来等级比较低

0 Kudos
Reply
10,410 Views
ydygcvjhbjkjnkn
Contributor I
你好,我们还没有企业邮箱,有企业微信,相关资料你可以通过企业微信发给我吗,企业微信收件箱:[email protected]
0 Kudos
Reply