FS26 unable to enter DFS State on KITFS26SKTEVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 unable to enter DFS State on KITFS26SKTEVM

1,227件の閲覧回数
RChatterjee
Contributor III

On programming FS26 using KITFS26SKTEVM Rev E, it is programmed in emulation mode with the following configuration (using FS26 GUI FS26):

1. Wake1 Event triggers DFS Exit

2. DFS Enable is set to when FS0B or RSTB is asserted.

In this mode, when RSTB is held low, even after more than 30s, the FS26 is not entering DFS mode.

Can such a functionality be tested when running in emulation?

PFA images of said configuration

ラベル(1)
0 件の賞賛
返信
1 返信

1,179件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

 

Had replied based on case 00621526

 

0 件の賞賛
返信