FS26 Safety Outputs release

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 Safety Outputs release

ソリューションへジャンプ
2,893件の閲覧回数
dingyazhou
Contributor I

Hello, I want to ask whether the fail-safe output release function Sbc_fs26_FsxbRelease of the FS26 chip needs to be called in a loop

0 件の賞賛
返信
1 解決策
2,775件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Yazhou,

It is necessary to write a 1 in order to clear the error flags bits. This is typically denoted in the FS26xx datasheet as “Clear on write to 1.”

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,888件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Yazhou,

There is no need to call this function in a loop to release FSxB.

The below diagram provides high level flow chart to enter Normal mode in the application.

Figure 16.JPG

Best regards,

Tomas

0 件の賞賛
返信
2,792件の閲覧回数
dingyazhou1
Contributor I

Hello, I have another question, is our error flag register, such as FS_OVUV_REG_STATUS register is cleared after error clearance, or do you need to manually write "1" software?

0 件の賞賛
返信
2,776件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Yazhou,

It is necessary to write a 1 in order to clear the error flags bits. This is typically denoted in the FS26xx datasheet as “Clear on write to 1.”

Best regards,

Tomas

0 件の賞賛
返信