FS26 - RSTB Path Check

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 - RSTB Path Check

1,473件の閲覧回数
wolfbiker1
Contributor I

Hi,

 

I am struggling doing FS26 RSTB Path check. How can I determine if the device boots up from cold start or from the reset injected with RSBT_REQ? (See SBC_FS26_FS_SAFE_IOS_1_ADDR Register)

 

I did some comparisons of those bits, cold start vs. rstb req but they are all similar.

 

Any suggestions here?

 

Thanks.

0 件の賞賛
返信
3 返答(返信)

1,405件の閲覧回数
wolfbiker1
Contributor I

Hello, may I have a quick update on my previous question? Thanks!

0 件の賞賛
返信

1,452件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Benjamin,

When the device starts from POR, BATTERY fail will be set (WUEVENT[3:0] = 0b1111).

For RSTB_REQ, this is requested by MCU, so the MCU knows this action, no register bits indicate it.

When there is external RSTB, RSTB_EVENT bit will be set. 

BRs, Tomas

0 件の賞賛
返信

1,445件の閲覧回数
wolfbiker1
Contributor I

Hi Tomas,

 

thank you very much for your response. As written in the data sheet I don't have the BAT_FAIL bit, but there is a BATTERY fail bit in M_WIO_FLG register at position WUEVENT[3:0]. All bits are always 0, any suggestions on that? May it regard with the debug mode of the SBC? 

Best,
Benjamin

0 件の賞賛
返信