FS23 INIT CRC error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FS23 INIT CRC error

822 次查看
Leex
Contributor I

 When I was debugging the system functions of FS23 +S32K3x, I found that if the INIT configuration of FS23 in my application program was inconsistent with that of FS23 in the Bootloader program, then when the system woke up from FS23 LPOFF mode, An INIT registers CRC error occurs in the FS233 initialization of both the Bootloader program and the application, causing the FS23 initialization to fail. In addition, if the POR (power on reset) is normal, this situation will not occur. How can I solve this proble

Leex_0-1729502647806.png

 

0 项奖励
回复
2 回复数

791 次查看
Leex
Contributor I

Leex_0-1729601592483.png

When an exception occurs, I find that INIT CRC error is raised whenever CRC is written

0 项奖励
回复

783 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Each time you exit the INIT phase, before that, you should confirm the INIT CRC value is written and the value is correct. 

Please refer the FS23 AN in secure files to understand the procedure. 

By the way, I can provide one file which can calculate the INIT CRC, but I cannot share it here, please open a support ticket.

0 项奖励
回复