Difference between MC33771B between MC33771C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between MC33771B between MC33771C

Jump to solution
2,199 Views
Ulli
Contributor I

Hi, there are different data sheets for the B suffix and C suffix of this device. But I could not find a difference between the C and the B, or a table of features to look this up. Where can I find this information?

0 Kudos
Reply
1 Solution
2,194 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Ulli,

The MC33771C is a successor of the MC33771B. The MC33771C offers an averaging functionality and improved communication. Other functions are not changed. The MC33771C is pin and package compatible to the MC33771B.

MC33771C improvements:

  • Averaging of up to 256 samples possible
  • Potential reduction in the diagnostic filtering time from 25 to 6 ms
  • Inductive and capacitive coupling support (current transformers & current external components)
  • Improved communication protocol
  • Up to 63 nodes are supported in one daisy chain
  • Supports 20 m cable length between two nodes with transformer isolation
  • Loopback support for one daisy chain

 

If you need more information about the differences between these devices, please submit a new case as it is confidential information.

I hope this information helps. 

Regards,

David

View solution in original post

0 Kudos
Reply
2 Replies
2,195 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Ulli,

The MC33771C is a successor of the MC33771B. The MC33771C offers an averaging functionality and improved communication. Other functions are not changed. The MC33771C is pin and package compatible to the MC33771B.

MC33771C improvements:

  • Averaging of up to 256 samples possible
  • Potential reduction in the diagnostic filtering time from 25 to 6 ms
  • Inductive and capacitive coupling support (current transformers & current external components)
  • Improved communication protocol
  • Up to 63 nodes are supported in one daisy chain
  • Supports 20 m cable length between two nodes with transformer isolation
  • Loopback support for one daisy chain

 

If you need more information about the differences between these devices, please submit a new case as it is confidential information.

I hope this information helps. 

Regards,

David

0 Kudos
Reply
2,193 Views
Ulli
Contributor I

Thank you for your help David! Much appreciated!

0 Kudos
Reply