Core Power Down Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Core Power Down Issue

5,296件の閲覧回数
schougule01
Contributor I

I am facing issue while loading script in the debugger.

I am getting "Core Power Down" issue while try to load script.

Is there any way to turn ON the Core Power to UP.

Controller: S32K148core_powereed down.png

タグ(1)
0 件の賞賛
返信
5 返答(返信)

5,273件の閲覧回数
schougule01
Contributor I

Hi,

@danielmartynekactually there is no issue in script as it works for other hardware.

0 件の賞賛
返信

5,262件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @schougule01,

Do you mean it works with other S32K148 MCUs?

Since I can't reproduce it, I would like to test you script on my side.

 

https://www2.lauterbach.com/pdf/error.pdf

danielmartynek_0-1678871528969.png

 

Is the VDD powered?

 

Regards,

Daniel

 

0 件の賞賛
返信

5,277件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @schougule01,

If the MCU powered, can you measure the VDD?

Can you please share the script?

 

Thanks,

BR, Daniel

0 件の賞賛
返信

5,253件の閲覧回数
rweiss
Contributor V

This error message usually means that the core's power domain in the SoC is not enabled. If the whole SoC is not powered, the error message would be "target power down" and the debugger would usually display "power down" in the status bar.

Detection of "Core Power Down" is not 100% reliable, depending on the SoC it could simply mean "could not communicate with core", with disabled power domain being the most typical reason.

Regards,
Reinhard

0 件の賞賛
返信

5,251件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @schougule01,

Can you catch it right after POR?

system.CPU S32K148
wait state.power()
system.attach

 

BR, Daniel

0 件の賞賛
返信