Confirmation of how to use the PCA9956B driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Confirmation of how to use the PCA9956B driver

2,614 次查看
m-kamijo
Contributor I

Although this PCA9956B driver can handle LED drive voltages up to 20v, for example, if one LED is connected to one pin and two series connections are connected to the other pin, it is possible to use a single unit and a single unit. Can you expect similar behavior for both series connections?
We will wait for the answer.

// LED spec //

Vf 2.0v

If 20mA

2019/06/20

I wonder if it was something like this?

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

2,405 次查看
m-kamijo
Contributor I

It was saved. Thank you very much.

0 项奖励
回复

2,404 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Could you please give me your application Block diagram ?

0 项奖励
回复

2,404 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

About your application block there is no problem!

0 项奖励
回复