Confirmation of how to use the PCA9956B driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Confirmation of how to use the PCA9956B driver

2,580 Views
m-kamijo
Contributor I

Although this PCA9956B driver can handle LED drive voltages up to 20v, for example, if one LED is connected to one pin and two series connections are connected to the other pin, it is possible to use a single unit and a single unit. Can you expect similar behavior for both series connections?
We will wait for the answer.

// LED spec //

Vf 2.0v

If 20mA

2019/06/20

I wonder if it was something like this?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,371 Views
m-kamijo
Contributor I

It was saved. Thank you very much.

0 Kudos
Reply

2,370 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Could you please give me your application Block diagram ?

0 Kudos
Reply

2,370 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

About your application block there is no problem!

0 Kudos
Reply