CANopen communication error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CANopen communication error

1,929 Views
saluguvenkat
Contributor I

CANopen communication I am getting the following error, can anybody explain which part is telling error message and error register here.

COBID: 601h
Message sent:          2B 60 60 00 01   (I am changing the operation mode to PP)
Error msg received:  80 60 60 00 12 00 07 06
 
Error code:
Error register:
and the rest of the field.
0 Kudos
Reply
1 Reply

1,850 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Can you please share more details about your application? For example, you don't mentioned which NXP part number you are using, this is needed to understand the problem and try to solve it.

Thanks,

Jose

0 Kudos
Reply