CANopen communication error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CANopen communication error

1,960件の閲覧回数
saluguvenkat
Contributor I

CANopen communication I am getting the following error, can anybody explain which part is telling error message and error register here.

COBID: 601h
Message sent:          2B 60 60 00 01   (I am changing the operation mode to PP)
Error msg received:  80 60 60 00 12 00 07 06
 
Error code:
Error register:
and the rest of the field.
0 件の賞賛
返信
1 返信

1,881件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

Can you please share more details about your application? For example, you don't mentioned which NXP part number you are using, this is needed to understand the problem and try to solve it.

Thanks,

Jose

0 件の賞賛
返信