CAN transceiver TJA1145 register initial values

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN transceiver TJA1145 register initial values

跳至解决方案
1,280 次查看
NxpCustomer
Contributor I

Hi,

What are the INIT values of registers in CAN transceivers TJA1145T and TJA1145AT? I am particularly interested in the following:

1. System event status register (address 61h)

2. CAN control register (address 20h)

3. Lock control register (address 0Ah)

In their datasheets, I could find descriptions of each of the bits of these registers, but not the Initial values. Also, INIT values of "reserved bits" could not be found.

Best regards,

Sharath

标记 (1)
0 项奖励
回复
1 解答
1,268 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You can check them in datasheet Table31--Table 31. Register bit settings in TJA1145A operating modes

在原帖中查看解决方案

2 回复数
1,163 次查看
NxpCustomer
Contributor I

Although I still do not find the value of reserved bits in Table31, this is good enough for me. Thank you very much! 

0 项奖励
回复
1,269 次查看
guoweisun
NXP TechSupport
NXP TechSupport

You can check them in datasheet Table31--Table 31. Register bit settings in TJA1145A operating modes