CAN transceiver TJA1145 register initial values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN transceiver TJA1145 register initial values

Jump to solution
1,275 Views
NxpCustomer
Contributor I

Hi,

What are the INIT values of registers in CAN transceivers TJA1145T and TJA1145AT? I am particularly interested in the following:

1. System event status register (address 61h)

2. CAN control register (address 20h)

3. Lock control register (address 0Ah)

In their datasheets, I could find descriptions of each of the bits of these registers, but not the Initial values. Also, INIT values of "reserved bits" could not be found.

Best regards,

Sharath

Tags (1)
0 Kudos
Reply
1 Solution
1,263 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can check them in datasheet Table31--Table 31. Register bit settings in TJA1145A operating modes

View solution in original post

2 Replies
1,158 Views
NxpCustomer
Contributor I

Although I still do not find the value of reserved bits in Table31, this is good enough for me. Thank you very much! 

0 Kudos
Reply
1,264 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can check them in datasheet Table31--Table 31. Register bit settings in TJA1145A operating modes