Are FS8530 and VR5500 100% compatible except functional safety features ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are FS8530 and VR5500 100% compatible except functional safety features ?

Jump to solution
3,776 Views
BL_
Contributor III

Hi NXP experts,

 

for the shake of simplicity in the current stage of our project, we want to replace the FS8530 PMIC by the VR5500 PMIC so that the functional safety aspects (e.g. watchdog feature) need not to be considered right now.

And the question is:

Are the FS8530 PMIC and the VR5500 PMIC 100% compatible except for functional safety features? I.e.

  • Regulator outputs compatible ?
  • Pin compatible ?
  • Design compatible ?

 

Thanks very much for your support.

BL

  •  
Tags (1)
0 Kudos
Reply
1 Solution
3,767 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you also have information regarding the following two points ?

1:Regulator outputs compatible ?

[gw]Regulators are compatible.

 

2:and Design compatible ?

[gw]VR5500 doesn't have FCCU and FS8530 has 4 channels of VMONx but VR500 onlh has one channel.

View solution in original post

0 Kudos
Reply
3 Replies
3,772 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please see below picture I attached for FS85/VR5500,red circle are the different points:

guoweisun_14-1648717215002.png

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

0 Kudos
Reply
3,770 Views
BL_
Contributor III

Hi Guoweisun,

thanks very much for the information about the Pin-compatible.

Do you also have information regarding the following two points ?

  • Regulator outputs compatible ? and
  • Design compatible ?

 

Thanks,

BL

 

0 Kudos
Reply
3,768 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you also have information regarding the following two points ?

1:Regulator outputs compatible ?

[gw]Regulators are compatible.

 

2:and Design compatible ?

[gw]VR5500 doesn't have FCCU and FS8530 has 4 channels of VMONx but VR500 onlh has one channel.

0 Kudos
Reply