Are FS8530 and VR5500 100% compatible except functional safety features ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are FS8530 and VR5500 100% compatible except functional safety features ?

ソリューションへジャンプ
3,778件の閲覧回数
BL_
Contributor III

Hi NXP experts,

 

for the shake of simplicity in the current stage of our project, we want to replace the FS8530 PMIC by the VR5500 PMIC so that the functional safety aspects (e.g. watchdog feature) need not to be considered right now.

And the question is:

Are the FS8530 PMIC and the VR5500 PMIC 100% compatible except for functional safety features? I.e.

  • Regulator outputs compatible ?
  • Pin compatible ?
  • Design compatible ?

 

Thanks very much for your support.

BL

  •  
タグ(1)
0 件の賞賛
返信
1 解決策
3,769件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Do you also have information regarding the following two points ?

1:Regulator outputs compatible ?

[gw]Regulators are compatible.

 

2:and Design compatible ?

[gw]VR5500 doesn't have FCCU and FS8530 has 4 channels of VMONx but VR500 onlh has one channel.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,774件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please see below picture I attached for FS85/VR5500,red circle are the different points:

guoweisun_14-1648717215002.png

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

0 件の賞賛
返信
3,772件の閲覧回数
BL_
Contributor III

Hi Guoweisun,

thanks very much for the information about the Pin-compatible.

Do you also have information regarding the following two points ?

  • Regulator outputs compatible ? and
  • Design compatible ?

 

Thanks,

BL

 

0 件の賞賛
返信
3,770件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Do you also have information regarding the following two points ?

1:Regulator outputs compatible ?

[gw]Regulators are compatible.

 

2:and Design compatible ?

[gw]VR5500 doesn't have FCCU and FS8530 has 4 channels of VMONx but VR500 onlh has one channel.

0 件の賞賛
返信