Adding POR supervisor to PF3000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding POR supervisor to PF3000

1,274件の閲覧回数
ryanmartin
Contributor III

Hello, we would like to add a POR supervisor to the PF3000 PMIC circuit.  We are using Vin=5V (USB) and want to ensure the power rails come up > 100ms after the USB power is applied to the device to meet USB inrush current specifications.  We are using a coin cell battery on VSNVS, so VSNVS will always be ~ 3.0V.  Is there a reference design available on how to add a POR supervisor to the PWRON pin?

Thanks,

Ryan

0 件の賞賛
返信
1 返信

1,210件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Ryan,

 

Unfortunately, we do not have any reference design available on how to add a POR supervisor to the PWRON pin specifically for the PF3000 PMIC.

However, in different designs, we had handled the POR supervision using a standard voltage supervisor chip named CAT811R from Catalyst Semiconductor.

 

Consult CAT811R datasheet for details and check if it works for your application.

 

Hope this helps.

 

Regards,

Jose

NXP Semiconductors

0 件の賞賛
返信