3 questions about MC33PT2000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

3 questions about MC33PT2000

Jump to solution
1,380 Views
Doublemint
Contributor II

Dear NXP Engineers,
Greetings,
Our company is considering using the MC33PT2000AF chip for 'current closed loop' control of solenoid valves. In this regard, I have consulted the 'MC33PT2000' and 'KTPT2000FRDM6CUG' technical documents for reference. However, there are certain discrepancies between the two documents that have not resolved my confusion:
1.In the application scenario of 6cylinder3bank, there are six components—'C_MHS1, C_MHS2, C_MLS1, C_MLS2' and 'R_GSHS1, R_GSHS2'—present in the schematic of the kit board that are not found in the 'recommended applications' section of the datasheet. What role do these components play in the circuit? Can they be omitted?
2.The kit board's documentation only describes the driving capabilities of the MC33PT2000. Can we utilize the full functionality of the chip as described using the kit board?
3.If I do not have a fuel pump and the Vboost is generated by another voltage chip, do I still need to draw the schematic for the fuel pump and the DC-DC block, and connect the generated Vboost voltage to the Vboost pin?
Thank you very much for your assistance.
Doublemit
December 21, 2023

0 Kudos
Reply
1 Solution
1,372 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:都是DNP 就是没有焊接的意思

guoweisun_0-1703137422000.png

2:可以

3:用不到的可以不画

 

View solution in original post

0 Kudos
Reply
2 Replies
1,373 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:都是DNP 就是没有焊接的意思

guoweisun_0-1703137422000.png

2:可以

3:用不到的可以不画

 

0 Kudos
Reply
1,371 Views
Doublemint
Contributor II

好的,十分感谢。

0 Kudos
Reply