3 questions about MC33PT2000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

3 questions about MC33PT2000

ソリューションへジャンプ
2,275件の閲覧回数
Doublemint
Contributor II

Dear NXP Engineers,
Greetings,
Our company is considering using the MC33PT2000AF chip for 'current closed loop' control of solenoid valves. In this regard, I have consulted the 'MC33PT2000' and 'KTPT2000FRDM6CUG' technical documents for reference. However, there are certain discrepancies between the two documents that have not resolved my confusion:
1.In the application scenario of 6cylinder3bank, there are six components—'C_MHS1, C_MHS2, C_MLS1, C_MLS2' and 'R_GSHS1, R_GSHS2'—present in the schematic of the kit board that are not found in the 'recommended applications' section of the datasheet. What role do these components play in the circuit? Can they be omitted?
2.The kit board's documentation only describes the driving capabilities of the MC33PT2000. Can we utilize the full functionality of the chip as described using the kit board?
3.If I do not have a fuel pump and the Vboost is generated by another voltage chip, do I still need to draw the schematic for the fuel pump and the DC-DC block, and connect the generated Vboost voltage to the Vboost pin?
Thank you very much for your assistance.
Doublemit
December 21, 2023

0 件の賞賛
返信
1 解決策
2,267件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1:都是DNP 就是没有焊接的意思

guoweisun_0-1703137422000.png

2:可以

3:用不到的可以不画

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,268件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1:都是DNP 就是没有焊接的意思

guoweisun_0-1703137422000.png

2:可以

3:用不到的可以不画

 

0 件の賞賛
返信
2,266件の閲覧回数
Doublemint
Contributor II

好的,十分感谢。

0 件の賞賛
返信