iMXRT1170EVKB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMXRT1170EVKB

2,106 次查看
KKR231
Contributor II

In iMX RT 1170 EVKB i got this problem during debugging.

Probe Firmware: MCU-LINK on-board (r0E2) CMSIS-DAP V2.250 (NXP Semiconductors)

Serial Number: NVUYDXEI5YUN1

VID:PID: 1FC9:0143

USB Path: \\?\hid#vid_1fc9&pid_0143&mi_00#7&38ddcd02&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}

connection failed - Em(04). Cannot provide power to DAP bus... Retrying

Failed on connect: Em(04). Cannot provide power to DAP bus.

Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>

Last stub error 0: OK

Last sticky error: 0x0 AIndex: 0

No debug bus (MemAp) selected

DAP Speed test unexecuted or failed

Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.

 

 

 

 

How can I solve it??

标记 (1)
0 项奖励
回复
1 回复

2,062 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

It is possible that the system is not powered correctly, if only using the debugger USB then you need to make sure that the jumper is on the correct position so it powers the entire system.
If everything is properly powered then refer to this post: RT board recovery for debugger connect issues - NXP Community

Best regards,
Omar

0 项奖励
回复