spi protocol sequence in P2040

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

spi protocol sequence in P2040

3,178 Views
gouravjain
Contributor IV

Hello All,

Can any one pls let me know about the configuration sequence of SPI protocol initialization in P2040 chipset. Since i want to write FPGA code (slave) which is connected to P2040 chipset on SPI bus.

regards,

Gourav

Labels (1)
0 Kudos
Reply
5 Replies

2,830 Views
ufedor
NXP Employee
NXP Employee

It is possible to refer to the QorIQ P2040 Reference Manual, 14.6 eSPI programming examples and U-Boot eSPI source code "u-boot/drivers/spi/fsl_espi.c" (u-boot/fsl_espi.c at 503eff00a7119d2690a662ed64e83e4782b7d3d9 · qoriq-open-source/u-boot · GitHub )

0 Kudos
Reply

2,830 Views
gouravjain
Contributor IV

Log when i'm trying to write in flash device(slave),

=> sf write 1000000 5 16
GJ: In SPI driver spi_claim_bus
spi_claim_bus: bus:0 cs:0
GJ: CSMODE[0]: 0x28170008
GJ: In SPI driver spi_xfer
spi_xfer: slave 0:0 dout 00000000(00000000) din 00000000(00000000) len 1
GJ: In SPI driver spi_cs_activate
GJ: command value 0x0
GJ: event_tx value: 0x208900
***spi_xfer:...06fa03ec written
GJ: event_rx value: 0x11dcb00
***spi_xfer:...00000000 readed
GJ: In SPI driver spi_xfer
GJ: In SPI driver spi_xfer
spi_xfer: slave 0:0 dout 00000000(00000000) din 00000000(00000000) len 23
GJ: In SPI driver spi_cs_activate
GJ: command value 0x16
GJ: event_tx value: 0x208900
***spi_xfer:...02000005 written
GJ: event_rx value: 0x420ab00
***spi_xfer:...00000000 readed
GJ: event_tx value: 0x208900
***spi_xfer:...02020202 written
GJ: event_rx value: 0x420ab00
***spi_xfer:...00000000 readed
GJ: event_tx value: 0x208900
***spi_xfer:...02010101 written
GJ: event_rx value: 0x420ab00
***spi_xfer:...00000000 readed
GJ: event_tx value: 0x208900
***spi_xfer:...fffffffd written
GJ: event_rx value: 0x420ab00
***spi_xfer:...00000000 readed
GJ: event_tx value: 0x208900
***spi_xfer:...fffffffc written
GJ: event_rx value: 0x420ab00
***spi_xfer:...00000000 readed
GJ: event_tx value: 0x208900
***spi_xfer:...ffffffec written
GJ: event_rx value: 0x31fcb00
***spi_xfer:...00000000 readed
GJ: In SPI driver spi_xfer
GJ: In SPI driver spi_xfer
spi_xfer: slave 0:0 dout 00000000(00000000) din 00000000(00000000) len 2
GJ: In SPI driver spi_cs_activate
GJ: command value 0x1
GJ: event_tx value: 0x208900
***spi_xfer:...05fa03ec written
GJ: event_rx value: 0x21ecb00
***spi_xfer:...00000000 readed
GJ: In SPI driver spi_xfer

As per mu understanding first time SPITF:06fa03ec --> first byte(06) is command for write enable rest didn't get

                                         Second time SPITF:02000005 --> first byte (02) is command for Page Program, rest for address(000005)

                                         Then several times SPITF will hold the transfer data until gets over.

                                         And finally last time SPITF: 05fa03ec --> first byte (05) command byte for read status register and rest bytes didn't understand.

Pls let me know if my understanding is wrong.

0 Kudos
Reply

2,830 Views
gouravjain
Contributor IV

Hi Ufedor,

Waiting for your reply....

0 Kudos
Reply

2,830 Views
gouravjain
Contributor IV

Hi,

In uboot when i do , sf probe 0

i found the below prints, (given some addition prints starting with GJ)

=> sf probe 0
GJ: SPI probed
cs value : 0
gj_temp1 value : 1
GJ: In SPI driver spi_claim_bus
spi_claim_bus: bus:0 cs:0
GJ: CSMODE[0]: 0x28170008
GJ: In SPI driver spi_xfer
GJ: In SPI driver spi_xfer
spi_xfer: slave 0:0 dout 00000000(00000000) din 00000000(00000000) len 6
GJ: In SPI driver spi_cs_activate
GJ: command value 0x5
GJ: event_tx value: 0x208900
***spi_xfer:...9ffa03f4 written
GJ: event_rx value: 0x420ab00
***spi_xfer:...00012018 readed
GJ: event_tx value: 0x208900
***spi_xfer:...18fa03f4 written
GJ: event_rx value: 0x21ecb00
***spi_xfer:...4d010101 readed
SF: Got idcodes
00000000: 01 20 18 4d 01 . .M.
SF: Detected S25FL129P_64K/S25FL128S with page size 64 KiB, total 16 MiB.

Not able to understand the highlighted part.

0 Kudos
Reply

2,830 Views
gouravjain
Contributor IV

Hi,

Thanks for you reply...

Just went through the section 14.6, and i'm not able to understand how to use  SPITF register.

Let's say i want to write 0x10 in slave in that case what would be the value of SPITF register??

0 Kudos
Reply