qcvs ddr config screen : field <skew clk to dqs>

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qcvs ddr config screen : field <skew clk to dqs>

2,760 Views
stefanvranken
Contributor II

Is this length-difference [mm] per bytelane between CLK-trace  and DQS[0:7]-trace ?
Or should I enter DQS-trace length [mm] ?

Labels (2)
Tags (3)
0 Kudos
Reply
2 Replies

2,455 Views
stefanvranken
Contributor II

Hello Pavel,
I think this number "skew CLK-to-DQS[0:7] in mm" to be entered in QCVS-ddr-tool is used to calculate the value of field WRLVLSTART in ddr-controller registers DDR_WRLVL_CNTL2/3 ?

Register DDR_WRLVL_CNTL has field WRTLVLSTART for DQS[0] I assume because P2020 reference manual shows just DQS here without [0] ?
WRLVLSTART for DQS[1 to 8] are in regs DDR_WRLVL_CNTL2 & 3.

Wite-levelling mechanism adjusts DQS-launch per bytelane (step 1/8 clk) to reach valid DQS - CLK timing a each dram-chip. Why is it necessary to have a WRLVLSTART value ? If I manually specify value 0000 then writelevelling starts searching over its entire range and will find adjustment value also ?

Does write-levelling overrule parameter WR_DAT_DELAY in register Timing_cfg_2 bits[19:21] ?  <<< Yes, see P2020RM page-385, Table 8-82, bit WRLVL_EN

WR_DAT_DELAY = wr-command to write-dq-dqs timing adjust = 1 clock delay   <<< my setting generated from QCVS-ddr-config

Regards, Stefan

0 Kudos
Reply

2,455 Views
Pavel
NXP Employee
NXP Employee

Look at the AN2582 about DDR layout rules:

http://cache.nxp.com/docs/en/application-note/AN2582.pdf?fsrch=1&sr=1&pageNum=1

 

See also AN2910:

http://cache.nxp.com/docs/en/application-note/AN2910.pdf?fsrch=1&sr=1&pageNum=1

 

and the AN5097:

http://cache.nxp.com/docs/en/application-note/AN5097.pdf?fsrch=1&sr=1&pageNum=1


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply