p2041 srio test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

p2041 srio test

跳至解决方案
2,049 次查看
yinux
Contributor III

hello,

      I can communicate between the 2 p2041 using the rapidIO.

     how can I using the message END API ?

       vxworks6.9

0 项奖励
回复
1 解答
1,780 次查看
Pavel
NXP Employee
NXP Employee
Yes, the P2041 can be connected using RapidIO. The P2041 can communicate using this connection. See please the Chapter 4.12 of the RapidIO Interconnect Specification, Revision 2.1 Part 6 (http://www.rapidio.org/specs/current)
 
There is single limitation for the P2041 and P4080 RapidIO:
The P2041 and P4080 RapidIO endpoint cannot be configured as four 1x ports

See also the following information on NXP Technical Information Centre for RapidIO testing:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-F7A5F5BE-3F93-4F6D-88...

See also the following Application Note: AN2923, AN2932 on Application Note.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,781 次查看
Pavel
NXP Employee
NXP Employee
Yes, the P2041 can be connected using RapidIO. The P2041 can communicate using this connection. See please the Chapter 4.12 of the RapidIO Interconnect Specification, Revision 2.1 Part 6 (http://www.rapidio.org/specs/current)
 
There is single limitation for the P2041 and P4080 RapidIO:
The P2041 and P4080 RapidIO endpoint cannot be configured as four 1x ports

See also the following information on NXP Technical Information Centre for RapidIO testing:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-F7A5F5BE-3F93-4F6D-88...

See also the following Application Note: AN2923, AN2932 on Application Note.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,780 次查看
yinux
Contributor III

got it ,thanks I will try.

0 项奖励
回复