p2041 srio test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,050件の閲覧回数
yinux
Contributor III

hello,

      I can communicate between the 2 p2041 using the rapidIO.

     how can I using the message END API ?

       vxworks6.9

ラベル(3)
0 件の賞賛
返信
1 解決策
1,781件の閲覧回数
Pavel
NXP Employee
NXP Employee
Yes, the P2041 can be connected using RapidIO. The P2041 can communicate using this connection. See please the Chapter 4.12 of the RapidIO Interconnect Specification, Revision 2.1 Part 6 (http://www.rapidio.org/specs/current)
 
There is single limitation for the P2041 and P4080 RapidIO:
The P2041 and P4080 RapidIO endpoint cannot be configured as four 1x ports

See also the following information on NXP Technical Information Centre for RapidIO testing:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-F7A5F5BE-3F93-4F6D-88...

See also the following Application Note: AN2923, AN2932 on Application Note.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,782件の閲覧回数
Pavel
NXP Employee
NXP Employee
Yes, the P2041 can be connected using RapidIO. The P2041 can communicate using this connection. See please the Chapter 4.12 of the RapidIO Interconnect Specification, Revision 2.1 Part 6 (http://www.rapidio.org/specs/current)
 
There is single limitation for the P2041 and P4080 RapidIO:
The P2041 and P4080 RapidIO endpoint cannot be configured as four 1x ports

See also the following information on NXP Technical Information Centre for RapidIO testing:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-F7A5F5BE-3F93-4F6D-88...

See also the following Application Note: AN2923, AN2932 on Application Note.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,781件の閲覧回数
yinux
Contributor III

got it ,thanks I will try.

0 件の賞賛
返信