a problem when bitbake devel-image(p4080pcie)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

a problem when bitbake devel-image(p4080pcie)

934 次查看
shanfeifei
Contributor II

According to release-notes-sdk-1.0.pdf,when i was building the image of  p4080pcie on ubuntu 14.04,there came a problem as followed:

freescale@freescale-sdk:~/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-

systembuilder$  bitbake devel-image

NOTE: Psyco JIT Compiler (http://psyco.sf.net) not available. Install it to increase performance.

NOTE: Handling BitBake files: \ (0394/0394) [100 %]

Parsing of 394 .bb files complete (388 cached, 6 parsed). 521 targets, 1 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

NOTE: preferred version 2010.12 of u-boot not available (for item u-boot)

NOTE: Preparing runqueue

NOTE: Executing runqueue

NOTE: Running task 605 of 1738 (ID: 1526, /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/oe-core/recipes/db/db_5.0.21.bb, do_compile)

NOTE: Running task 608 of 1738 (ID: 1487, /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/sb-core/recipes/binutils/binutils-oprofile_2.20.1.bb, do_compile)

NOTE: package db-5.0.21-r1: task do_compile: Started

ERROR: TaskFailed event exception, aborting

ERROR: Build of /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/oe-core/recipes/db/db_5.0.21.bb do_compile failed

ERROR: Task 1526 (/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/oe-core/recipes/db/db_5.0.21.bb, do_compile) failed with 256

ERROR: Function do_compile failed

NOTE: Task failed: ('function do_compile failed', '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/db-5.0.21-r1/temp/log.do_compile.2837')

ERROR: Logfile of failure stored in: /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/db-5.0.21-r1/temp/log.do_compile.2837

Log data follows:

| NOTE: make -j 4

| ./libtool --mode=link powerpc-linux-gnu-gcc -mcpu=e500mc -maix-struct-return --sysroot=/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux -fexpensive-optimizations -frename-registers -fomit-frame-pointer -O2 -g0  -o db_archive -L/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-rpath-link,/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-O1 -Wl,--hash-style=gnu -B/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib \

|    db_archive.lo util_sig.lo libdb-5.0.la -lpthread

| ./libtool --mode=link powerpc-linux-gnu-gcc -mcpu=e500mc -maix-struct-return --sysroot=/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux -fexpensive-optimizations -frename-registers -fomit-frame-pointer -O2 -g0  -o db_checkpoint -L/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-rpath-link,/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-O1 -Wl,--hash-style=gnu -B/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib \

|    db_checkpoint.lo util_log.lo util_sig.lo libdb-5.0.la -lpthread

| ./libtool --mode=link powerpc-linux-gnu-gcc -mcpu=e500mc -maix-struct-return --sysroot=/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux -fexpensive-optimizations -frename-registers -fomit-frame-pointer -O2 -g0  -o db_deadlock -L/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-rpath-link,/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-O1 -Wl,--hash-style=gnu -B/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib \

|    db_deadlock.lo util_log.lo util_sig.lo libdb-5.0.la -lpthread

| ./libtool --mode=link powerpc-linux-gnu-gcc -mcpu=e500mc -maix-struct-return --sysroot=/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux -fexpensive-optimizations -frename-registers -fomit-frame-pointer -O2 -g0  -o db_dump -L/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-rpath-link,/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-O1 -Wl,--hash-style=gnu -B/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib \

|    db_dump.lo util_cache.lo util_sig.lo libdb-5.0.la -lpthread

| libtool: link: powerpc-linux-gnu-gcc -mcpu=e500mc -maix-struct-return --sysroot=/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux -fexpensive-optimizations -frename-registers -fomit-frame-pointer -O2 -g0 -o .libs/db_dump -Wl,-rpath-link -Wl,/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-O1 -Wl,--hash-style=gnu -B/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib .libs/db_dump.o .libs/util_cache.o .libs/util_sig.o  -L/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib ./.libs/libdb-5.0.so -lpthread

| libtool: link: powerpc-linux-gnu-gcc -mcpu=e500mc -maix-struct-return --sysroot=/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux -fexpensive-optimizations -frename-registers -fomit-frame-pointer -O2 -g0 -o .libs/db_deadlock -Wl,-rpath-link -Wl,/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-O1 -Wl,--hash-style=gnu -B/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib .libs/db_deadlock.o .libs/util_log.o .libs/util_sig.o  -L/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib ./.libs/libdb-5.0.so -lpthread

| libtool: link: powerpc-linux-gnu-gcc -mcpu=e500mc -maix-struct-return --sysroot=/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux -fexpensive-optimizations -frename-registers -fomit-frame-pointer -O2 -g0 -o .libs/db_checkpoint -Wl,-rpath-link -Wl,/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-O1 -Wl,--hash-style=gnu -B/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib .libs/db_checkpoint.o .libs/util_log.o .libs/util_sig.o  -L/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib ./.libs/libdb-5.0.so -lpthread

| libtool: link: powerpc-linux-gnu-gcc -mcpu=e500mc -maix-struct-return --sysroot=/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux -fexpensive-optimizations -frename-registers -fomit-frame-pointer -O2 -g0 -o .libs/db_archive -Wl,-rpath-link -Wl,/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib -Wl,-O1 -Wl,--hash-style=gnu -B/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib .libs/db_archive.o .libs/util_sig.o  -L/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/sysroots/ppce500mc-linux/usr/lib ./.libs/libdb-5.0.so -lpthread

| ./.libs/libdb-5.0.so: undefined reference to `__txn_getactive'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_regop_42_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_stat_print_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_ckp_desc'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_ckp_42_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_closeevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_tx_max'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_region_mutex_count'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_init_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_create'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_refresh'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_findlastckp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_reset'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remrem'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_tx_timestamp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_lockevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_begin'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_tx_timestamp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_applied_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_failchk'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_activekids'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_open'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_recycle_id'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_record_fname'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_begin_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_recover_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_force_abort'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_getckp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remlock'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_commit'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remove_buffer'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_abort'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_tx_max'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_destroy'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_stat_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_checkpoint'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_oldest_reader'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_checkpoint_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_preclose'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_add_buffer'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_name'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_timeout'

| collect2: ld returned 1 exit status

| ./.libs/libdb-5.0.so: undefined reference to `__txn_getactive'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_regop_42_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_stat_print_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_ckp_desc'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_ckp_42_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_closeevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_tx_max'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_region_mutex_count'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_init_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_create'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_refresh'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_findlastckp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_reset'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remrem'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_tx_timestamp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_lockevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_begin'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_tx_timestamp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_applied_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_failchk'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_activekids'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_open'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_recycle_id'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_record_fname'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_begin_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_recover_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_force_abort'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_getckp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remlock'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_commit'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remove_buffer'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_abort'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_tx_max'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_destroy'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_stat_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_checkpoint'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_oldest_reader'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_checkpoint_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_preclose'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_add_buffer'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_name'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_timeout'

| collect2: ld returned 1 exit status

| ./.libs/libdb-5.0.so: undefined reference to `__txn_getactive'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_regop_42_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_stat_print_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_ckp_desc'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_ckp_42_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_closeevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_tx_max'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_region_mutex_count'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_init_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_create'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_refresh'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_findlastckp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_reset'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remrem'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_tx_timestamp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_lockevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_begin'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_tx_timestamp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_applied_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_failchk'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_activekids'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_open'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_recycle_id'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_record_fname'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_begin_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_recover_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_force_abort'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_getckp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remlock'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_commit'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remove_buffer'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_abort'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_tx_max'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_destroy'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_stat_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_checkpoint'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_oldest_reader'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_checkpoint_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_preclose'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_add_buffer'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_name'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_timeout'

| collect2: ld returned 1 exit status

| make: *** [db_dump] Error 1

| make: *** Waiting for unfinished jobs....

| make: *** [db_deadlock] Error 1

| ./.libs/libdb-5.0.so: undefined reference to `__txn_getactive'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_regop_42_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_stat_print_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_ckp_desc'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_ckp_42_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_closeevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_tx_max'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_region_mutex_count'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_init_recover'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_create'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_refresh'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_findlastckp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_reset'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remrem'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_tx_timestamp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_lockevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_begin'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_tx_timestamp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_applied_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_failchk'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_activekids'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_open'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_recycle_id'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_record_fname'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_begin_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_recover_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_force_abort'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_getckp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remlock'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_commit'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remove_buffer'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_abort'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_tx_max'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_env_destroy'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_stat_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_remevent'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_checkpoint'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_oldest_reader'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_checkpoint_pp'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_preclose'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_add_buffer'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_get_name'

| ./.libs/libdb-5.0.so: undefined reference to `__txn_set_timeout'

| collect2: ld returned 1 exit status

| make: *** [db_archive] Error 1

| make: *** [db_checkpoint] Error 1

| FATAL: oe_runmake failed

| ERROR: Function do_compile failed

NOTE: package db-5.0.21-r1: task do_compile: Failed

ERROR: TaskFailed event exception, aborting

ERROR: Build of /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/oe-core/recipes/db/db_5.0.21.bb do_compile failed

ERROR: Task 1526 (/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/oe-core/recipes/db/db_5.0.21.bb, do_compile) failed with 256

Waiting for 1 active tasks to finish:

1: binutils-oprofile-2.20.1-r0.2 do_compile (pid 2838)

NOTE: package binutils-oprofile-2.20.1-r0.2: task do_compile: Started

ERROR: TaskFailed event exception, aborting

ERROR: Build of /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/sb-core/recipes/binutils/binutils-oprofile_2.20.1.bb do_compile failed

ERROR: Function do_compile failed

NOTE: Task failed: ('function do_compile failed', '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/temp/log.do_compile.2838')

ERROR: Logfile of failure stored in: /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/temp/log.do_compile.2838

Log data follows:

| NOTE: make -j 4 configure-build-libiberty all

| make[1]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux'

| make[1]: Nothing to be done for `all-target'.

| make[2]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/intl'

| make[2]: Nothing to be done for `all'.

| make[2]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/intl'

| make[2]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/libiberty'

| make[2]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/etc'

| for f in standards.info configure.info; do \

|  if test -f /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/etc/`echo $f | sed -e 's/.info$/.texi/'`; then \

|    if make "MAKEINFO=makeinfo --split-size=5000000 --split-size=5000000" $f; then \

|      true; \

|    else \

|      exit 1; \

|    fi; \

|  fi; \

| done

| make[3]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/libiberty/testsuite'

| make[3]: Nothing to be done for `all'.

| make[3]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/libiberty/testsuite'

| make[2]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/libiberty'

| make[3]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/etc'

| make[3]: `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/etc/standards.info' is up to date.

| make[3]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/etc'

| make[3]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/etc'

| make[3]: `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/etc/configure.info' is up to date.

| make[3]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/etc'

| make[2]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/etc'

| make[2]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/bfd'

| Making info in doc

| make[3]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/bfd/doc'

| restore=: && backupdir=".am$$" && \

| rm -rf $backupdir && mkdir $backupdir && \

| if (makeinfo --split-size=5000000 --split-size=5000000 --version) >/dev/null 2>&1; then \

|  for f in bfd.info bfd.info-[0-9] bfd.info-[0-9][0-9] bfd.i[0-9] bfd.i[0-9][0-9]; do \

|    if test -f $f; then mv $f $backupdir; restore=mv; else :; fi; \

|  done; \

| else :; fi && \

| if makeinfo --split-size=5000000 --split-size=5000000   -I /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/bfd/doc \

| -o bfd.info `test -f 'bfd.texinfo' || echo '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/bfd/doc/'`bfd.texinfo; \

| then \

|  rc=0; \

| else \

|  rc=$?; \

|  $restore $backupdir/* `echo "./bfd.info" | sed 's|[^/]*$||'`; \

| fi; \

| rm -rf $backupdir; exit $rc

| /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/bfd/doc/bfd.texinfo:326: unknown command `colophon'

| /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/bfd/doc/bfd.texinfo:337: unknown command `cygnus'

| make[3]: *** [bfd.info] Error 1

| make[3]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/bfd/doc'

| Making info in po

| make[3]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/bfd/po'

| make[3]: Nothing to be done for `info'.

| make[3]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/bfd/po'

| make[3]: Entering directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/bfd'

| make[3]: Nothing to be done for `info-am'.

| make[3]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/bfd'

| make[2]: *** [info-recursive] Error 1

| make[2]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux/bfd'

| make[1]: *** [all-bfd] Error 2

| make[1]: Leaving directory `/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/build_p4080n710_release/work/ppce500mc-linux/binutils-oprofile-2.20.1-r0.2/binutils-2.20.1/build.powerpc-linux.powerpc-linux'

| make: *** [all] Error 2

| FATAL: oe_runmake failed

| ERROR: Function do_compile failed

NOTE: package binutils-oprofile-2.20.1-r0.2: task do_compile: Failed

ERROR: TaskFailed event exception, aborting

ERROR: Task 1487 (/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/sb-core/recipes/binutils/binutils-oprofile_2.20.1.bb, do_compile) failed with 256

ERROR: '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/oe-core/recipes/db/db_5.0.21.bb' failed

ERROR: '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/sb-core/recipes/binutils/binutils-oprofile_2.20.1.bb' failed

ERROR: Build of /home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/sb-core/recipes/binutils/binutils-oprofile_2.20.1.bb do_compile failed

ERROR: Task 1487 (/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/sb-core/recipes/binutils/binutils-oprofile_2.20.1.bb, do_compile) failed with 256

ERROR: '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/oe-core/recipes/db/db_5.0.21.bb' failed

ERROR: '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/sb-core/recipes/binutils/binutils-oprofile_2.20.1.bb' failed

ERROR: '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/oe-core/recipes/db/db_5.0.21.bb' failed

ERROR: '/home/freescale/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder/sb-core/recipes/binutils/binutils-oprofile_2.20.1.bb' failed

freescale@freescale-sdk:~/P4080-PCIE-SDK-1.0-05-03-2012/QorIQ-DPAA-SDK-20110609-systembuilder$

标签 (1)
0 项奖励
回复
1 回复

719 次查看
Pavel
NXP Employee
NXP Employee

This SDK was developed for Ubuntu 8.04 and Ubuntu 10.04.

Test shows that this SDK cannot build image under Ubuntu 14.

Use Ubunu 10.04 for this SDK. There is no problem if Ubuntu 10.04 is used.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复