What are the differences between processors having different PVRs?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What are the differences between processors having different PVRs?

跳至解决方案
1,759 次查看
sissi_yang
Contributor I

Hi,all

      I want to konw the differences between processors having different PVRs.I kown PVR values contain information on both the cpu model(upper 16 bits) and on the precise revision(low 16 bits).But I want to know the exact attributes that may affect software.Like e500v2,for example.I want to emulate a e500v2 core using QEMU,the exact PVR is 0x80212051 and the QEMU doesn't support.I want to kown the attributes of the 0x80212051 to make some changes.Anyone can help me?Thank you.


标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,629 次查看
scottwood
NXP Employee
NXP Employee

I don't think we have a public document describing differences between revisions of a core.  However, I do not think the differences would be relevant to QEMU -- usually they are bug fixes or things which are not software-visible.  You could add it as a new PVR (CPU_POWERPC_e500v2_v51_dp would be an appropriate name) but no behavioral differences.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,630 次查看
scottwood
NXP Employee
NXP Employee

I don't think we have a public document describing differences between revisions of a core.  However, I do not think the differences would be relevant to QEMU -- usually they are bug fixes or things which are not software-visible.  You could add it as a new PVR (CPU_POWERPC_e500v2_v51_dp would be an appropriate name) but no behavioral differences.

0 项奖励
回复
1,629 次查看
sissi_yang
Contributor I

Thank you very much!

0 项奖励
回复