Using MPIC when CPC is set as SRAM P4080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using MPIC when CPC is set as SRAM P4080

Jump to solution
1,288 Views
hymalaibello
Contributor III

Hello,

I am using the CPC as SRAM, and I would like to know whether I can  use the MPIC (Multicore Programmable Interrupt Controller) while the SRAM configuration is enabled?

Thanks!!

Regards,

Hymalai Bello

Labels (1)
0 Kudos
Reply
1 Solution
1,126 Views
LPP
NXP Employee
NXP Employee

MPIC can be used without any relation to CPC mode.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,127 Views
LPP
NXP Employee
NXP Employee

MPIC can be used without any relation to CPC mode.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply