Using MPIC when CPC is set as SRAM P4080

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using MPIC when CPC is set as SRAM P4080

ソリューションへジャンプ
1,822件の閲覧回数
hymalaibello
Contributor III

Hello,

I am using the CPC as SRAM, and I would like to know whether I can  use the MPIC (Multicore Programmable Interrupt Controller) while the SRAM configuration is enabled?

Thanks!!

Regards,

Hymalai Bello

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
1,660件の閲覧回数
LPP
NXP Employee
NXP Employee

MPIC can be used without any relation to CPC mode.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,661件の閲覧回数
LPP
NXP Employee
NXP Employee

MPIC can be used without any relation to CPC mode.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信