Using MPIC when CPC is set as SRAM P4080

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using MPIC when CPC is set as SRAM P4080

跳至解决方案
1,271 次查看
hymalaibello
Contributor III

Hello,

I am using the CPC as SRAM, and I would like to know whether I can  use the MPIC (Multicore Programmable Interrupt Controller) while the SRAM configuration is enabled?

Thanks!!

Regards,

Hymalai Bello

标签 (1)
0 项奖励
回复
1 解答
1,109 次查看
LPP
NXP Employee
NXP Employee

MPIC can be used without any relation to CPC mode.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,110 次查看
LPP
NXP Employee
NXP Employee

MPIC can be used without any relation to CPC mode.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复