The remote emulator cannot touch P2020 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The remote emulator cannot touch P2020 processor

1,556件の閲覧回数
rainbowyang
Contributor I

Hi,

    I have designed a board using P2020 processor,at first the board worked well,but then i changed the hardware design in the 2th edition,i have updated the board using a diffierent CPLD,which provides the power-on logic control.There's no other changes.I found that the processor cannot be in the 'ready' state,it always be in the 'asleep' state.Would you please tell me what i should do next?Thanks very much!

ラベル(1)
0 件の賞賛
返信
1 返信

1,450件の閲覧回数
ufedor
NXP Employee
NXP Employee

You have to check what is wrong with the CPLD logic.

It is needed to refer to the P2020 QorIQ Integrated Processor Reference Manual, 4.5.2 Power-on reset sequence and P2020 QorIQ Integrated Processor Hardware Specifications, 2.5 RESET Initialization.

0 件の賞賛
返信