The remote emulator cannot touch P2020 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The remote emulator cannot touch P2020 processor

1,600 次查看
rainbowyang
Fresh Out Contributor

Hi,

    I have designed a board using P2020 processor,at first the board worked well,but then i changed the hardware design in the 2th edition,i have updated the board using a diffierent CPLD,which provides the power-on logic control.There's no other changes.I found that the processor cannot be in the 'ready' state,it always be in the 'asleep' state.Would you please tell me what i should do next?Thanks very much!

标签 (1)
0 项奖励
回复
1 回复

1,494 次查看
ufedor
NXP Employee
NXP Employee

You have to check what is wrong with the CPLD logic.

It is needed to refer to the P2020 QorIQ Integrated Processor Reference Manual, 4.5.2 Power-on reset sequence and P2020 QorIQ Integrated Processor Hardware Specifications, 2.5 RESET Initialization.

0 项奖励
回复