Security Engine inside P5040

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Security Engine inside P5040

ソリューションへジャンプ
1,604件の閲覧回数
weizhao
Contributor I

Hi,

We're using P5040 QorIQ Integrated Multicore Communication Processor in our products.  According to P5040 manual, there is a security engine inside P5040, and we'd like to use i as Random Number Generator.  Is there any application note for the security engine using ?

Thanks,

Wei

0 件の賞賛
返信
1 解決策
1,440件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

There is separate P5040 Security (SEC) Reference Manual on the P5040 web page

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

There are application notes for the SEC 2.0 and SEC 3.x but it is not so useful because the P5040 has SEC rev. 4.2. You can search for the security training courses on the NXP site. For example see “Introduction to Security Acceleration in QorIQ Processors”

https://community.nxp.com/servlet/JiveServlet/downloadBody/331881-102-1-267794/DES-N1856%20Security%...

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,441件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

There is separate P5040 Security (SEC) Reference Manual on the P5040 web page

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

There are application notes for the SEC 2.0 and SEC 3.x but it is not so useful because the P5040 has SEC rev. 4.2. You can search for the security training courses on the NXP site. For example see “Introduction to Security Acceleration in QorIQ Processors”

https://community.nxp.com/servlet/JiveServlet/downloadBody/331881-102-1-267794/DES-N1856%20Security%...

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信