SDK crossscripts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK crossscripts

2,039件の閲覧回数
dan
Contributor I

We currently have two teams working on development for the P4040.  We are using two different compile machines.

What I have found is that when the they ran bitbake fsl-image-full the following file was modified with their paths

build_p4080ds_release/tmp/sysroots/p4080ds/usr/bin/crossscripts/powerpc-fsl-linux-libtool

On the build system that I am using, no matter what bitbake recipe I use, this file never gets modified.  All of the paths are prefixed /home/jenkins.  We are both currently using SDK 1.2.1.  Any thoughts on why this file is not getting modified?  I am getting ready to manually edit it.

ラベル(1)
0 件の賞賛
返信
1 返信

1,916件の閲覧回数
mattsm
Contributor III

Are you both using the sstate-cache provided ISO?

-M

0 件の賞賛
返信