SDK crossscripts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK crossscripts

2,080 Views
dan
Contributor I

We currently have two teams working on development for the P4040.  We are using two different compile machines.

What I have found is that when the they ran bitbake fsl-image-full the following file was modified with their paths

build_p4080ds_release/tmp/sysroots/p4080ds/usr/bin/crossscripts/powerpc-fsl-linux-libtool

On the build system that I am using, no matter what bitbake recipe I use, this file never gets modified.  All of the paths are prefixed /home/jenkins.  We are both currently using SDK 1.2.1.  Any thoughts on why this file is not getting modified?  I am getting ready to manually edit it.

Labels (1)
0 Kudos
Reply
1 Reply

1,957 Views
mattsm
Contributor III

Are you both using the sstate-cache provided ISO?

-M

0 Kudos
Reply