SATA init issues on P5020 with kernel 3.17-rc3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SATA init issues on P5020 with kernel 3.17-rc3

3,556 次查看
RabbitHoleComp
Contributor II

        Has anyone here successfully built and booted a recent kernel from mainline? I have one built, however upon boot, sata init fails. Are there any known SATA-related erratum that I should be patching for?

标签 (1)
0 项奖励
回复
7 回复数

3,135 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Alex Perez,

Would you please provide your u-boot and Kernel boot log?

What is the revision of P5020 used?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,135 次查看
RabbitHoleComp
Contributor II

yipingwang

Sure, I can provide a kernel boot log. The P5020 I am using is production/shipping silicon. If you can tell me how to verify (via /proc or similar mechanism) which version it is, I'll be happy to double-check.

0 项奖励
回复

3,135 次查看
scottwood
NXP Employee
NXP Employee

U-Boot prints the SoC version in the boot messages.

0 项奖励
回复

3,135 次查看
scottwood
NXP Employee
NXP Employee

In Custom kernel for T4240qds - boot issues you said that the patches I linked to resolved your SATA problems -- are there any remaining issues?

0 项奖励
回复

3,135 次查看
RabbitHoleComp
Contributor II

scottwood, I see that the necessary SATA patches have made it in to mainline as of 3.18, however as previously stated, I have a machine which (using both 3.17-rc3 AND 3.18.1, does not enumerate any PCI devices on the tree. Are there any known patchsets to resolve this?

0 项奖励
回复

3,135 次查看
scottwood
NXP Employee
NXP Employee

Please post a new topic for the PCI issue, with a boot log and other relevant information.

0 项奖励
回复

3,135 次查看
RabbitHoleComp
Contributor II

Yes, those patches definitely resolve my SATA issues, however no PCI devices are enumerating on the bus (lspci returns nothing)

As for silicon revision, I am at 2.0:

U-Boot 2014.04-00110-g021fb01-dirty (Aug 20 2014 - 12:43:46)

CPU0:  P5020, Version: 2.0, (0x82200020)

Core:  e5500, Version: 1.2, (0x80240012)

0 项奖励
回复