P5020 Absolute Maximum Operating Temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P5020 Absolute Maximum Operating Temperature

3,034 Views
ethan135
Contributor II

Does NXP have any limits or data on the absolute maximum operating temperature of the P5020 processor? 

The hardware manual states the maximum recommended operating temperature is +105C but what happens if this is exceeded while operating but below the non-operational temperature maximum (+150C) for a period of less than a week?

0 Kudos
Reply
4 Replies

2,966 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ethan,

Thank you so much for provide the entire part number,

I have checked with the team and please note if you do not follow the specs and requirements that has been tested and supported located on the data sheet of the QorIQ P5020/P5010 Data
Sheet, 
In the long run you may damage the device of find unexpected errors.

Have a Wonderful day.

Best regards,

Hector Villarruel.

 

 

0 Kudos
Reply

2,977 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ethan,

Could you please be so kind to provide the entire part number nomenclature of the device?

We will be waiting for your kind update,

Best Regards,

Hector Villarruel.

0 Kudos
Reply

2,973 Views
ethan135
Contributor II

Hi Hector,

Thanks for taking a look at this.  The entire NXP part number is: P5020NXE7QMB

Regards,
Ethan

0 Kudos
Reply

2,994 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello Ethan,

This post is to inform you that we are still working to answer your questions about this case.

I will keep you informed.

BR,

Hector

0 Kudos
Reply